Command 'Resolve conflict' Permalink

Symbol: _svn_icon_compare

Function: This command opens the “<object>” dialog. In the dialog, the conflicts are displayed and functions for resolving conflicts are prepared in order to merge changes.

Call: Context menu of the object.

Requirement: The object has a conflict that has occurred by updating the object with local changes.

Dialog '<object>'

“Compare”

The local objects are displayed on the left side, and the version from the SVN repository is displayed on the right side.

“Use mine”

A local change is used.

“Use yours”

A change of the version from the SVN repository is changed.

“Apply”

All changes are accepted that you made in this dialog. The status of the object is changed.

“Cancel”

Cancels all changes that you made in this dialog. But the object keeps the conflicted status.