Command 'Clear authentication data' Permalink

Function: This command opens the “CODESYS” dialog. In this dialog, define the caches that will be deleted.

Call: Menu bar: “Project  SVN”.

Dialog 'CODESYS'

The authentication memory contains the authentication data of all SVN repositories for which the user has selected for saving the authorization data. This memory is deleted completely by this command.

“Clear the shared on-disk cache.”

_cds_icon_option_activated: The data saved on the computer is deleted.

“Clear the RAM cache of this instance.”

_cds_icon_option_activated: The data saved in the RAM is deleted.

The authentication data saved on the computer is stored in ‎%APPDATA%\Subversion\auth‎. This memory path is also used for most other Subversion client applications (for example, TortoiseSVN and AnkhSVN). Therefore, deleting the authentication data affects these applications as well.