Dialog 'Static Analysis Settings' - 'Settings'Permalink

Function: In the dialog, you select automatic static analysis, and save or load the project settings for static analysis as a CSA file.

Call:

  • Menu bar: “Project  Project Settings”, “Static Analysis” category, “Open configuration dialog” link

  • Menu bar: “Build  Static analysis  Settings”

Requirement:

  • The CODESYS Static Analysis package is installed.

  • A project is open.

“Perform static analysis automatically”

_cds_icon_option_activated: CODESYS performs the code check automatically at each code generation (for example, when the “Build  Generate Code” command is executed or before a download.

_cds_icon_option_deactivated: The code check is not performed automatically, but it can be performed explicitly by means of the “Build  Static Analysis  Run Static Analysis” command.

“Load”

Opens the “Load Static Analysis Configuration” dialog for selecting the project settings for the static analysis as a CSA file in the file system. When you click the “Open” button, the selected CSA file is loaded.

“Save”

Opens the “Save Static Analysis Configuration” dialog for saving all project settings in the “Static Analysis” category as a CSA file in the file system.