Dialog 'Static Analysis Settings' - 'Forbidden Symbols'Permalink

Function: In the dialog, you define the keywords and symbols that must not be used in the project code.

Call:

  • “Open configuration dialog” button in the menu “Project  Project Settings”, “Static Analysis” category

  • Menu bar: “Build  Static analysis  Settings”

Requirement:

  • The CODESYS Static Analysis package is installed.

  • A project is open.

Input line

Double-clicking the line opens the line editor for specifying a keyword or symbol.

_cds_icon_input_assistent: The Input Assistant opens for selecting the keyword or symbol.