Attribute 'analysis:report-multiple-instance-calls'Permalink

The attribute marks a function block for checking for rule 105: Only function blocks with this attribute are checked whether the function block instances are called more than one time. If rule 105 is deactivated in the project settings, then the attribute does not have any effect.

Insert location: Top line in the declaration part of a function block.

Syntax:

{attribute 'analysis:report-multiple-instance-calls'}

Example

// {attribute 'analysis:report-multiple-instance-calls'} Deactivated
FUNCTION_BLOCK FB_DoA
VAR_INPUT
END_VAR
VAR_OUTPUT
END_VAR
VAR
	iA : INT;
END_VAR
iA := iA + 1;

{attribute 'analysis:report-multiple-instance-calls'}
FUNCTION_BLOCK FB_DoB
VAR_INPUT
END_VAR
VAR_OUTPUT
END_VAR
VAR
	iB : INT;
END_VAR
iB := iB +1;

PROGRAM PLC_PRG
VAR
	fbA : FB_DoA;
	fbB : FB_DoB;
ND_VAR

fbA();
fbB();	// SA0105
fbA();
fbB();	// SA0105

--> SA0105: Instance 'fbB' called more than once