Tab: EtherCAT Slave – Process Data Permalink

The tab displays the process data of the slave inputs and outputs. The data is preset from the device description file.

Table 469: Select the Outputs

The table shows the slave outputs defined by “Start address”, “Type”, and “Index”.

If device outputs are enabled for writing, they can be assigned to project variables in the “EtherCAT I/O Mapping” dialog.

Table 470: Select the Inputs

The table shows the slave inputs defined by “Name”, “Type”, and “Index”.

If device inputs are enabled for reading, they can be assigned to project variables in the “EtherCAT I/O Mapping” dialog.