The tab provides a more detailed view of the process data that is also displayed in the “Process Data” dialog. In addition, PDO assignment and PDO configuration can be downloaded on this tab.
Requirement: Expert settings are enabled for the slave.
|
List of Sync Managers with data size and PDO type. |
|
List of PDOs assigned to the selected “Sync-Manager”. |
|
|
When a check box is selected, the corresponding PDOs are enabled and I/O channels are created. This is similar to the simplified PDO configuration view. |
|
List of PDOs assigned to the selected “Sync-Manager”. |
|
|
Entries can be added, edited, or deleted using the corresponding commands (“Add”, “Delete”, “Edit”) in the command bar or context menu. |
|
“Name” |
|
|
“Index” |
|
|
“Direction” |
|
|
“Flags” |
|
|
“Exclude PDOs” |
It is possible to define an exclusion list. When a PDO is enabled in the “PDO assignment”, others are disabled and cannot be enabled. |
|
“Sync unit” |
ID of the Sync Manager to which the PDO is to be assigned. |
|
Displays the contents of the PDOs selected in the “PDO list”. Entries can be added, edited, or deleted using the corresponding commands (“Add”, “Delete”, “Edit”) in the command bar or context menu. The PDO order can be changed using “Move Up” and “Move Down”. |
|
“PDO assignment” |
|
|
“PDO configuration” |
|
|
“Load PDO info from the device” |
The current PDO configuration is read from the slave and entered into the configuration. The lists in the upper and lower right are then deleted and filled with the read data. This is especially useful when the ESI file is incomplete and the configuration is available only on the slave. |
: The PDO is transmitted from the master to the slave.