Getting Started with Trend Recording Permalink

To execute trend recording on a runtime system, you need an application with a “Trend Recording Manager” object that contains at least one “Trend Recording” object. Then you can configure a database on the runtime system and the data buffering.

Getting Started

  1. Add a “Trend Recording Manager” object below your application.

  2. Select the “Trend Recording Manager” object and click “Add Object  Trend Recording”. Type a name in the “Add Trend Recording” dialog.

    The object is created and the editor opens.

  3. Type a time interval in “Record Settings”.

  4. Click “Add Variable”.

    An additional variable has been added. The blank settings open in the “Variable Settings” to the right of the tree view.

  5. Select a valid IEC variable from the “Variable” field.

    The IEC variable is configured for trend recording.

  6. Build the application.

  7. Download the application to the controller and click “Start”.

    The application records data at runtime and saves it to a database.