Configuring the Project Settings Permalink

You can configure settings that affect the behavior of CODESYS and that of certain editors in the “Project Settings” object. The settings are valid throughout the project and are applied immediately for active editors. You can also use the “Project  Project Settings” command to access the dialogs of the object.

CODESYS saves the project settings as an object within the project. Then when you transfer a project to another system, the “Project Settings” object is transferred with it. There is no need for a project archive.