Enabling the security features Permalink

First switch the communication to encryption so that you do not reveal any credentials to other participants in the network when transferring the user management.

Enforcing encrypted communication

  • On the controller

    • Runtime version >= 3.5 SP14: Encryption can be enabled for “Communication Policy” and enforced for all clients.

  • In CODESYS

    • Encrypted communication can be selected as an option in the device editor on the “Communication Settings” tab (command or “Change Communication Policy” dialog) or in the “Security Screen” view.

      For more information, see: ⮫ “Encrypting Communication, Changing Security Settings ”

      If the CODESYS Security Agent is installed, then see the help for CODESYS Security Agent.

Enforcing a user management