Option: --ignoreproperties (ignore object properties in project comparison) Permalink

If you add this option after the option ‎--compare <project1> <project2>‎, then object properties (permissions, compile settings, directories, bitmaps, etc.) are ignored in the project comparison.

Syntax:

--compare="<path of project file>" "<path of reference project file>" --ignoreproperties="true"|"false"

Example

Automation Builder.exe --compare "D:\proj\project1.project" "D:\proj\project2.project" --ignoreproperties="true"