Special methods of a function block Permalink

‎FB_Init‎

Declarations automatically implicit, but explicit declaration also possible

Contains initialization code for the function block, as is defined in the declaration part of the function block

‎FB_Reinit‎

Explicit declaration is necessary.

Call after the instance of the function block was copied (as during an online change). It reinitializes the new instance module.

‎FB_Exit‎

Explicit declaration is necessary.

Call for each instance of the function block before a new download or a reset or during an online change for all shifted or deleted instances.

⮫ Properties

Provides ‎Set‎ and/or ‎Get‎ accessor methods.