Object: DeviceTrace Permalink

Symbol: _visu_icon_trace.png

A “DeviceTrace” object shows trace data in one or more diagrams, as does a “Trace” object.

The difference is that a “DeviceTrace” directly ⮫ accesses traces that are running on the controller. The object is inserted below the device in the device tree. Therefore there is no immediate dependency on the applications in the CODESYS project.

ou can use the DeviceTrace to display in a visualization the processor load of a "multicore" controller. For more information on "Multicore" see: ⮫ Multicore

For more information about the editor and its operation, see the help page for the ⮫ Trace object.