Hiding windows Permalink

When you hide a view, it is minimized to a tab in the frame of the user interface. When you hover the pointer over the tab, the window is shown automatically.

  1. Click in the window which you want to hide.

  2. Select the “Window  Auto Hide” option.

    Or click the _cds_icon_hide.png symbol in the upper right corner of the view.

    The window is hidden and visible by means of a small tab located in the edge of the main window.

  3. Move the mouse pointer over the tab.

    The window is shown as long as the mouse pointer hovers over the tab.