This dialog is intended for test purposes. Its values should be changed only by experts.
The device-specific parameters are displayed in a table on this tab of the generic device editor. The device description defines which parameters you can edit in this dialog.
You can sort the entries in alphabetically ascending or descending order or in the default order by clicking the column header.
|
“Parameter” |
Parameter name, not editable |
|
“Type” |
Data type of the parameter, not editable |
|
“Value” |
Initially displays the default value of the parameter, directly or the corresponding symbol name. Non-editable parameters are displayed in light-gray. If the parameter is editable you can open an input field, a drop-down list or a file selection dialog with a double-click the table field and use it to change the value. |
|
“Default value” |
Default value of the parameter defined by the device description, not editable |
|
“Unit” |
Unit of measure for the value (example: "ms" for milliseconds; not editable) |
|
“Description” |
Short description of the parameter specified by the device description, not editable |