Customizing Command Icons Permalink

CODESYS provides the capability of assigning customized icons to commands.

  1. Click “Tools  Customize”.

    The “Customize” dialog opens.

  2. Click the ⮫ Command Icons tab.

  3. In the overview on the left, select the “Help” category.

    All commands of this category are displayed on the right side.

  4. Click “Information”.

  5. Click the “Assign” button.

    A dialog opens for selecting the icon file (*.ico).

  6. Select an icon file.

  7. Click the “Open” button.

    The icon is assigned to the selected command.

  8. Click “OK”.