Command 'Replace', 'Replace in Project'Permalink

Symbol _cds_icon_replace; keyboard shortcut: [Ctrl]+[H]

Symbol _cds_icon_replace_in_project, keyboard shortcut [Ctrl]+[Shift]+[H]

Function: These commands scan the project or parts of it for a specified character string and replaces it.

Call: Menu bar: “Edit  Find Replace”

Requirement: The application is in online mode.

This command opens the “Replace” dialog where the search and replace character strings are specified and the search options are defined.

Table 624: In addition to the options of the “Search” dialog, the following settings are still possible:

“Replace with”

Input field for the new character string.

“Replace”

Each next found string is highlighted in the editor and replaced (step-by-step replace).

“Replace all”

All found strings are replaced at one time without them being displayed in the editors.

“Leave changed objects open after "Replace all"”

The editors of the found objects remain open.

Replacement in referenced libraries is not possible.