Command 'Refactoring' - 'Reorder Variables'Permalink

Symbol: _cds_icon_refactoring_reorder

Function: This command allows changing the order of variables in the declaration editor for the selected scope: ‎VAR_INPUT‎, ‎VAR_OUTPUT‎, or ‎VAR_IN_OUT‎.

Call: “Edit  Refactoring”; context menu of the focused scope in the declaration editor.

Requirement: One of the above scopes is selected in the declaration, and more than one variable is declared in it.

The command opens the “Reorder” dialog box with a list of all declarations of the selected scope. You can drag a selected declaration up or down to another position.

See also