Command: Refactoring – Add Variable Permalink

Symbol: _cds_icon_refactoring_add_variable.png

Function: The command allows for the declaration of variables in a POU, as well as the automatic update to the occurrence locations of the POU.

Call: “Edit  Refactoring” menu; context menu

Requirement: The declaration part is in focus.

The command opens the default dialog for declaring variables.