Command: Load Core Dump Permalink

Function: CODESYS scans the project directory for core dump files. When a new core dump is forced with the “Create Core Dump” command, the core dump file is automatically loaded from the controller to the project directory. If multiple core dump files are available, then CODESYS prompts you to choose whether or not the last generated file should be opened in the project. Alternatively, you could also select one of the other files.

When a file is loaded into the project, an online view of the application is displayed with state of the application at the time when the core dump was generated. There you can view the variable values afterwards. The call tree is also available there.

Call: “Debug  Core Dump” menu

Requirement: The application is in offline mode.

NOTICE

NOTICE
NOTICE
NOTICE

NOTICE

NOTICE

You can close the core dump view only by clicking “Close Core Dump”. The “Logout” command has no effect in this view.

For more information, see: ⮫ “Performing an Error Analysis with Core Dump ” and ⮫ “Command: Create Core Dump ”