Command 'Insert Text'Permalink

Symbol: icon_insert_text

Function: This command inserts a new line into the text list above the selected line. An input field under “Standard” opens, in which you input the source text.

Call: Main menu “Textlist  Insert Text”, context menu

Requirement: A text list, not a “GlobalTextList”, is open and active. A field in the table is selected.

See also