Command 'Go to Instance'Permalink

Symbol: _cds_icon_goto_instance

Function: This command opens the instance of a function block in a new window.

Call: Menu bar: “Edit  Browse for Symbol”

Requirement: The application is in online mode. A POU is open in the editor and the cursor is at an instance of a function block.

The command is not available for temporary instances or instances from compiled libraries.

See also