Command 'Check Library Compatibility'Permalink

Function: The command triggers a check whether the currently opened library project is compatible with the last installed version of this library (next lower version number) .

Call: By default the command is not available in any menu. You can add it to a menu by using the “Tools  Customize” dialog, command category “Build”.

Requirement: A library project is opened.

The check regards differences in the implemented interfaces of a method. So, after the check you will get displayed error messages in the messages window in the following cases:

  • Adding or removing inputs or outputs of function blocks, functions or methods

  • Changing the data type of inputs or outputs

  • Modifying the implemented interfaces of a method

See also