Command 'Set Start of Feedback'Permalink

Symbol: _cds_icon_start_of_feedback

Function: The command defines the selected element as the starting point within a feedback.

Call:

  • Menu bar: “CFC  Execution Order”

  • Context menu: “Execution Order”

Requirement: A CFC editor is active and the “Auto Data Flow Mode” property is selected. Moreover, a network of the CFC POU contains a feedback, and an element within the feedback is selected.

In the CFC editor, the starting point within the feedbacks is decorated with the _cds_icon_start_of_feedback symbol. Then the element has the lowest number in the execution order within the feedbacks. At runtime, the processing of the feedback begins with this element.