Command: S (Set) Permalink

Symbol: cfc_icon_set.png, Shortcut: [Ctrl]+[M] (to toggle between “S”, “R”, “REF”, and none)

Function: The command adds a Set (S) to the input of a Boolean “Output” element.

Call: “CFC → Set/Reset” menu; context menu

Requirement: A CFC editor is active. The input of an “Output” element is selected.

If an “Output” element has a Set input, then the Boolean output value is set to “TRUE” as soon as the value of the input is “TRUE”. The “TRUE” value at the output is retained, even if the input value changes.