Command: None Permalink

Symbol: cfc_icon_none.png, Shortcut: [Ctrl]+[M] (to toggle between “S”, “R”, “REF”, and none)

Function: The command removes a Reset (R), Set (S), or REF from the input of the “Output” element.

Call: “CFC  Set/Reset” menu, “Set/Reset” in the context menu

Requirement: A CFC editor is active. The input of an “Output” element is selected.