Command 'Prepare Box for Forcing'Permalink

This command is required when using compiler versions 3.5.11.x and 3.5.12.x. The command is no longer required for compiler versions >= 3.5.13.0.

Function: The command activates and deactivates the forceability of the inputs for a function block element.

Call:

  • CFC

  • Context menu

Requirements: The CFC editor is in offline mode and a function block element is selected.

After executing the command, the “Force Function Block Input” command is available in online mode to open a dialog for forcing the box input values.