Command 'Edit Worksheet'Permalink

Function: This command opens the “Edit Worksheet” dialog box in which you set the size of the worksheet.

Call: Main menu “CFC”

Requirements: A CFC editor is active.

Dialog box 'Edit worksheet'

“Use following dimensions”

Here is where you set the size of the worksheet. Your change is only accepted if the size is sufficient for the existing program.

“Adapt the dimensions automatically”

Automatically adapts the size of the worksheet to the size of your program.

“Move the working sheet origin relatively”

Shifts the worksheet along the x or y axis. The input of negative numbers is permitted.