Command: Create Control Point Permalink

Symbol: cfc_icon_create_control_point.png

Function: The command creates a control point at a connector.

Call: “SVN” in the context menu

Requirement: A CFC editor is active. The cursor is located over a connection.

The control point is created at the position on the connecting line where the cursor is located when the command is executed.

Alternatively, you could also drag a control point from the “ToolBox” view to the editor.