Command: Connect Selected Pins Permalink

Symbol: cfc_icon_connect_selected_pins.png

Function: The command establishes a connection between the selected ports.

Call: “CFC” menu; context menu

Requirement: A CFC editor is active. Exactly one output and multiple inputs are selected.

To select the ports, you have to hold down the [Ctrl] key while clicking the ports. After that, execute the command.