Changing the Window Layout Permalink

In CODESYS, you can easily customize the layout of different views to your individual needs.

  1. Drag the view by the title bar or by the tab.

    Arrows are shown to mark possible destinations. Example: _cds_img_window_position.png

  2. Drag the view to one of the arrows.

    The destination is displayed as a blue-shaded area.

  3. Release the left mouse button.

    The window is added in the selected target area.

The window can also be placed outside of the CODESYS programming interface.

For more information, see: ⮫ “Resizing Windows ”