Safety instructions and preconditions to use drives libraryPermalink

The user has to read the following instructions and documents before using the libraries:

  • All pertinent state, regional, and local safety regulations must be observed when installing and using this product. When functions or devices are used for applications with technical safety requirements, the relevant instructions must be followed.

  • Read the complete safety instructions of the user's manuals for the devices you are using, before installation and commissioning.

  • Read all safety instructions of the AC500 PLC. See System description AC500 in the online help in Automation Builder.

  • Read the user information of the devices and functions you are using, see online help in Automation Builder.

  • Installation and commissioning of the drive(s) is not part of this document nor the online help of Automation Builder. Installation and commissioning of the drive(s) must be done according to the related drives manuals and safety instructions.

The library package has been released for the software and firmware versions listed in the readme file of the package only.

In no event will ABB or its representatives be liable for loss of data, profits, revenue or consequential, incidental or other damage that may result from the use of other versions of product, software or firmware versions. The error-free operation of the Drives Library with other devices, software or firmware versions should be possible but cannot be guaranteed and may need adaptations e.g. of example programs.

The user must follow all applicable safety instructions and the guidelines mentioned in the user documents of the ABB products.

Read the complete safety instructions for the AC500 before installation and commissioning.

CAUTION

CAUTION
CAUTION
CAUTION

CAUTION

CAUTION

Generally, the user in all applications is fully and alone responsible for checking all functions carefully, especially for safe and reliable operation.

The function blocks contained in the library can only be executed in RUN mode of the PLC, but not in simulation mode.