RSPermalink

Provided by standard library.

Resetting bistable function blocks

Q1 = RS (SET, RESET1) means:

Q1 = NOT RESET1 AND (Q1 OR SET)

The input variables SET and RESET1 as well as the output variable Q1 are type BOOL.

Declaration example

RSInst : RS ;

Example in Function Block Digram

COD_RS

Example in Structured Text

RSInst(SET:= VarBOOL1 , RESET1:=VarBOOL2 );

VarBOOL3 := RSInst.Q1 ;