INSERTPermalink

Provided by standard ibrary.

INSERT inserts a string into another string at a defined point.

The input variables STR1 and STR2 are type STRING, POS is type INT and the return value of the function is type STRING.

INSERT(STR1, STR2, POS) means: insert STR2 into STR1 after position POS.

Example in Function Block Diagram

COD_INSERT

Example in Structured Text

VarSTRING1 := INSERT ('SUSI','XY',2);

String functions are not "thread safe": When using tasks, string functions may only be used in a single task. If the same function is used in different tasks, there is a danger of overwriting.