Symbol: 
The tab includes a list of configured keyboard shortcuts that are valid for all visualizations available throughout the application. Therefore, the tab is the central location for defining keyboard shortcuts for all visualizations that are below an application.
Keyboard shortcuts of the default keyboard action are not listed here.
The tab is similar to the “Keyboard Configuration” tab and provides the same editing options.
See also