Symbol: 
Function: This tab provides settings for adapting the font and font size in the visualization according to the language. The settings apply to all visualizations of the application, including the visualization manager.
|
“Language” |
Language used in the project. A column is created for each language. All text lists, including those from integrated libraries, are scanned for this. |
|
“Font” |
Font used by the visualization depending on the language. |
|
“Size factor” |
The factor affects the type size of all texts in the visualization. Preset: 1 If the factor is smaller than 1, this leads to a reduction of the type size. If the factor is 1, all texts are displayed unchanged as defined in “Properties”. |
|
Red highlighting of a cell |
The highlighted language is no longer present in the text lists of the project or the libraries. This highlighting is not available in runtime mode. |
|
Context menu of a selected table row |
|
|
“Delete Language” |
The associated column is removed. This is advisable above all if settings in the column are highlighted in red. |
|
“Copy Language Settings” |
All settings in the column are copied to the clipboard. |
|
“Paste Language Settings” |
All settings in the column are overwritten with the values from the clipboard. |
|
“Automatic decrease of font size” |
Tip: This prevents a text from being truncated when changing to a language that needs more space. The requirement is that a font is available which has a sufficiently small font. |
See also
: If the text to be displayed does not fit in the text field in the set format, then
the font size is decreased automatically until the text fits completely in the text
field.