Function: The dialog includes the configuration for the display settings of the trace diagram (for both the X-axis and Y-axis) and provides a preview in the trace diagram.
Call: “Display” button in “Trace Configuration” dialog.
|
“Add Y-Axis” |
Extends the trace diagram by one Y-axis. Result: The “Trace Configuration” dialog contains an extended selection of Y-axes in the “Additional axes” option of the variable settings. |
|
“Delete Y-axis” |
Deletes the Y-axis with the visible tab. |
Tab 'X-axis'
|
“Display Mode” |
Scaling
|
|
“Minimum” |
Initial value of the segment. Requirement: The “Display Mode” is “Fixed”. |
|
“Maximum” |
End value of the segment. Requirement: The “Display Mode” is “Fixed”. |
|
“Length” |
Constant length of the segment. |
|
“Grid” |
|
|
“Fixed spacing” |
|
|
“Distance” |
Distance between tick marks |
|
“Subdivisions” |
Number of subdivisions between two tick marks |
|
“Font” |
Font for the X-axis |
Tab 'Y-Axis'
|
“Display Mode” |
Scaling
|
|
“Minimum” |
Literal, variable (integer data type), or constant variable (integer data type). It contains the initial value of the segment. Requirement: The “Display Mode” is “Fixed”. Examples: Note: The variable has to have an initial value. This is important for the offline
display and the scaling subdivision. Example: |
|
“Maximum” |
Literal, variable (integer data type), or constant variable (integer data type). It contains the end value of the segment. Requirement: The “Display Mode” is “Fixed”. Examples: Note: The variable has to have an initial value. This is important for the offline
display and the scaling subdivision. Example: |
|
“Grid” |
|
|
“Label” |
|
|
“Fixed spacing” |
|
|
“Distance” |
Distance between tick marks |
|
“Subdivisions” |
Number of subdivisions between two tick marks |
|
“Font” |
Font for the Y-axis |
Preview of the trace diagram

|
“Background color” |
|
|
“Reset” |
CODESYS resets all settings to the defaults. |
|
“Use as default” |
CODESYS saves the settings as default |
: