Function: The recording rate of the “Trace” visualization element is configured in this dialog box.
Call
-
Properties: “Trace”
, “Advanced” -
Context menu: “Configure trace”, “Advanced”
Requirement: A trace is selected in the active visualization editor.
|
“Measurement in every nth cycle” |
The task where the trace is running is the basis for the measurement. The measurement interval is a multiple of the trace task according to the selected value. The measurement interval is displayed on the right side. |
|
“Buffer size (samples)”. |
The number of measurements is calculated according to the time range of the x-axis. |
See also