Function: The dialog displays the currently used visualization style of the project. The visualization style can be updated here.
Call: Main menu “Project Project Environment”, tab “Visualization Styles”
|
“For the following visualization styles currently in use, newer versions are available:” |
|
|
“Visualization Styles” |
Version of the currently set visualization style of the opened project. |
|
“Current” |
Current version of the visualization style, for example |
|
“Recommended” |
Recommenden version of the visualization style, for example |
|
“Action” |
|
|
“Do not update” |
The visualization style of the project remains unchanged. |
|
“Update to x.x.x.x” |
CODESYS updates the project to the version of the chosen visualization style. |
|
“ Check for updates when loading the project” |
|
|
“Set All to Newest” |
CODESYS updates the version. |
See also
:
: No check of the version. The update dialogs do not open automatically any longer.