Symbol:
Function: This command opens the “Visualization Styles” dialog box. It makes it possible to edit visualization style repositories.
Call: Menu bar: “Tools”.
Dialog Box 'Visualization Styles'
“Storage location” |
Name of the currently selected repository Preset: “System”
|
“(...)” |
Storage location of the repository Example: |
“Edit locations” |
The “Edit Repository Locations” dialog box opens. |
“Company” |
When a company name is specified here, the tree view is filtered and only the styles of the selected company are listed. Preset: “(All companies)”. It is not filtered.
|
Windows with styles |
Tree view of all versions of the installed visualization styles in the selected repository |
“Display localized names” |
|
“Install” |
The “Select Visualization Style(s)” dialog box opens. |
“Uninstall” |
The selected style version is removed from the repository. |
“Preview” |
The windows closes. A preview is displayed of the selected style in the selected version. Specific elements are displayed in the style. |
Dialog box 'Edit Repository Locations'
“Location” |
Storage location of the configured repository on the development system Example: |
“Name” |
Preset: |
“Add” |
The “Repository Locations” dialog box opens. It makes it possible to manage other repositories. |
“Edit” |
|
“Remove” |
|
“Move Up” |
The order in the list of repositories is adapted. It defines the processing order when searching for elements. |
“Move Down” |