Symbol: 
Function: This command activates and deactivates the keyboard usage when a visualization is executed in online mode (integrated in CODESYS).
Call: Menu bar: “Visualization”; context menu.
Requirement: A visualization is open.
When this command is active, the visualization executes the keyboard events that you specified as a visualization user.
When the command is inactive, CODESYS executes the keyboard events that you specify.
See also