Symbol: 
Function: The behavior of the integrated SVN version control system is configured in this dialog.
Call: Menu bar: “Project Project Settings” (“SVN Settings”).
Requirement: A project is open.
|
With these settings, you can overwrite the default settings that were made in the dialog “Tools Options”, category “SVN Settings”. |
|
|
“Merge” |
Behavior for the commands “Update”, “Merge”, or “Switch”, when both sides (working copy and SVN repository) have changed from the base version. |
|
“Locks” |
Behavior such as Professional Version Control objects when they are changed locally. |
|
“Marker” |
Behavior for conflicts |
|
“Create SVN_VERSION_INFO constants for IEC access” |
When you activate the option, the object is created automatically. When you deactivate the option, the object is removed from the project automatically. |
: The object
: The object