Symbol:
Function: This command opens the “SVN Properties” dialog. Here you can edit the properties of the versioned object.
Call: Context menu: “SVN”
Requirement: A versioned, unlocked object is selected.
Dialog 'SVN Properties'
“Name” |
Name of the property Example: Note: SVN has some reserved properties. Example: |
“Value” |
Example: Double-click in the field to edit the value. |
“Add” |
Opens a dialog to define another property with its value. |
“Remove” |
Deletes the selected property. |
“Show binary properties” |
|
“Reset” |
Resets the changes displayed in green. |
“OK” |
Accepts the changes. |
See also