Symbol: 
Function: This command opens the “Connect to SVN repository” dialog. In the dialog, you define the URL and the revision of the SVN repository with which the unversioned project is connected.
Call: Menu bar: “Project SVN”.
Requirement: The project is disconnected from SVN.




NOTICE

Only users who have read access to the entire project (see the CODESYS user and access management) can import the project into the SVN repository or can link to an existing database project.




NOTICE

This command functions reliably only when the project has already been imported into SVN and then disconnected with the command “Disconnect project from SVN”.
Dialog 'Connect to SVN repository'
|
“URL of existing project” |
URL of the SVN repository “HEAD”: Selection of the revision in the “Select revision” dialog
|
|
“Checkout options” |
“Omit externals”: External objects are not checked out. |
|
“Revision” |
|
See also
: Selection of the SVN repository in the
: Date display in universal time.