Object: EtherCAT Slave
The tab reads the diagnosis data (0x10f3 object) of the slave and displays it in a tree structure. Moreover, the messages
are issued in plain language.
Requirement: The application is in online mode. The attribute DiagHistory in the ESI file is set.
|
“Update history” |
The data is read again and the view is refreshed. New messages are displayed in the “Flags” column with “N” (New). Acknowledged messages with “Q”. |
|
“Auto update” |
The data is updated automatically. |
|
“New messages only” |
Acknowledged messages are not displayed. |
|
“Acknowledge messages” |
All messages with the “N” flag are acknowledged. Then the flag changes to “Q”. |
See also