Input variables are used at the inputs of function blocks.
VAR_INPUT variables are declared between the keywords VAR_INPUT and END_VAR in the declaration part of programming objects.
You can extend input variables with an attribute keyword.
Example
VAR_INPUT iIn1 : INT; (* 1st input variable *) END_VAR
See also