External variables are global variables that are imported into a block.
You declare these variables between the keywords VAR_EXTERNAL
and END_VAR
. If the global variable does not exist, then an error message is printed.




NOTICE

CODESYS does not require you to declare a global variable as external in order to use it in a POU. The keyword exists only for maintaining compliance with IEC 61131-3.
Syntax
<POU keyword> <POU name> VAR_EXTERNAL <variable name> : <data type>; END_VAR
Initialization is not permitted.
Example
FUNCTION_BLOCK FB_DoSomething VAR_EXTERNAL iVarExt1 : INT; (* 1st external variable *) END_VAR