The assignment operator => assigns the output of a function, a function block, or a method to a variable. The
position on the right side of the operator can also be blank.
Syntax
<output> => <variable>
Example
FBcomp_Output1 => bVar1; FBcomp_Output2 => ;
FBcom_Output1 and FB_Output2 are outputs of a function block. The value of FBcom_Output1 is assigned to the variable bVar1.