CODESYS provides the capability to display the events and error messages logged in the controller.
See also
Reading the log
Requirement: The controller is running.
-
Select the controller in the device tree.
-
Choose the command “Project Edit Object”.
The device editor opens.
-
Choose the tab “Log”.
-
Click on
to update the view.A connection to the controller is established. The controller in the device tree is highlighted in green.
All controller log information are displayed.
-
Click on
to delete the current list. -
Filter the view by clicking on the desired category (for example "Information").
-
Save the log entries. Click on
and choose a file name.
See also