The effect of this pragma is that a defined warning is displayed for a data type definition during compilation if the data type (structure, function block, etc.) is used in the project. This enables you, for example, to draw attention to the fact that a data type is no longer valid because, for example, an interface has changed and this should also be implemented in the project.
In contrast to a message pragma this warning is defined centrally for all instances of a data type.
Syntax:
{attribute 'obsolete' := 'user defined text'}
Insertion position: line of the data type definition or in a line above it.
Example
The pragma is inserted in the definition function block fb1
:
{attribute 'obsolete' := 'datatype fb1 not valid!'} FUNCTION_BLOCK fb1 VAR_INPUT i:INT; END_VAR
If you use fb1 as a data type, for example in fbinst:fb1
, the following warning will be displayed when compiling the project: "datatype fb1
not valid".
See also